AXIS#.HWEN.MODE
Description
Selects whether AXIS#.CLRFAULTS is performed on the rising edge
A rising edge is the transition of a digital signal from low to high. It is also called positive edge of the hardware enable input
Examples
Usage
0 (default): perform AXIS#.CLRFAULTS on the rising edge of the hardware enable input
1: do not perform clear faults on the rising edge of the hardware enable input
Code
--> AXIS1.HWEN.MODE 0
--> AXIS2.HWEN.MODE 1
Context
For more information on hardware enable, refer to the Enable/Disable.
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-00-00-000 |
General Information
| Type | Read/Write |
| Units | N/A |
| Range | 0 to 1 |
| Default Value | 0 |
| Data Type | Integer |
| See Also | AXIS#.HWEN.SOURCE, AXIS#.HWEN.STATE, AXIS#.CLRFAULTS |
|
Stored in Non Volatile Memory |
Yes |
Variants Supported
All variants are supported
Fieldbus Information
| Fieldbus |
Parameter | Index | Sub-Index | Data Type | Float Scale | Units | Access | PDO Mappable |
|---|---|---|---|---|---|---|---|---|
| EtherCAT |
AXIS1.HWEN.MODE | 0x5009 | 0x2 | USINT | - | - | RW | False |
| AXIS2.HWEN.MODE | 0x5109 | 0x2 | USINT | - | - | RW | False |
|
Copyright © 2018 Kollmorgen |
|